Write/Read |
About GCA Analysis |
Description |
Sets and returns whether the CW frequency for the compression analysis trace can be set to only the discrete frequencies or provides interpolation. |
VB Syntax |
gcaMeas.AnalysisIsDiscreteFreq = value |
Variable |
(Type) - Description |
|
gcaMeas |
A GainCompressionMeas (object) |
|
value |
(Boolean) Choose from: False - Interpolated data points. True - Discrete data points only. |
Return Type |
Boolean |
Default |
False |
Examples |
gcaMeas.AnalysisIsDiscreteFreq = True 'Write |
|
isDisc = gca.AnalysisIsDiscreteFreq 'Read |
|
C++ Syntax |
HRESULT get_AnalysisIsDiscreteFreq(VARIANT_BOOL* value) HRESULT put_AnalysisIsDiscreteFreq(VARIANT_BOOL value) |
Interface |
IGainCompressionMeas |