Write/Read |
About GCA Analysis |
Description |
Sets and returns the type of data to display on the x-axis of a compression analysis trace. |
VB Syntax |
gcaMeas.AnalysisXAxis = value |
Variable |
(Type) - Description |
|
gcaMeas |
A GainCompressionMeas (object) |
|
value |
(Enum as NAGCAAnalysisXAxis) Choose from: naPsourceAsXAxis (0) - Power from the source. naPinAsXAxis (1) - Input power to the DUT. |
Return Type |
Enum |
Default |
naPinAsXAxis (1) |
Examples |
gcaMeas.AnalysisXAxis = naPinAsXAxis 'Write |
|
xAxis = gca.AnalysisXAxis 'Read |
|
C++ Syntax |
HRESULT get_AnalysisXAxis(tagNAGCAAnalysisXAxis* value) HRESULT put_AnalysisXAxis(tagNAGCAAnalysisXAxis value) |
Interface |
IGainCompressionMeas |