Write/Read |
About ECAL orientation |
Description |
Sets ECAL module automatic orientation ON or OFF. |
VB Syntax |
obj.AutoOrient = bool |
Variable |
(Type) - Description |
|
obj |
SMCType (object) or VMCType (object) |
bool |
(Boolean) True - Set AutoOrientation ON False - Set AutoOrientation OFF |
Return Type |
Boolean |
Default |
True |
Examples |
Smc.AutoOrient = True |
C++ Syntax |
HRESULT put_AutoOrient(VARIANT_BOOL bAutoOrient); HRESULT get_AutoOrient(VARIANT_BOOL *bAutoOrient); |
Interface |
SMCType VMCType |