Write/Read |
About Auto Port Extensions |
Description |
Sets the frequency span that is used to calculate Automatic Port Extension. Learn more about calculating Automatic Port Extension. |
VB Syntax |
fixture.AutoPortExtConfig = value |
Variable |
(Type) - Description |
|
fixture |
A Fixturing (object) |
|
value |
(ENUM as NAAutoPortExtConfig) 0 naAPEC_CSPN - Use current span. 1 naAPEC_AMKR - Use active marker frequency. 2 naAPEC_USPN - Use custom user span. Use AutoPortExtSearchStart Property and AutoPortExtSearchStop Property to specify start and stop frequency. |
Return Type |
ENUM |
Default |
0 naAPEC_CSPN |
Examples |
fixture.AutoPortExtConfig = naAPEC_AMKR |
|
value = fixture.AutoPortExtConfig 'Read |
|
C++ Syntax |
HRESULT get_AutoPortExtConfig(tagNAAutoPortExtConfig *pVal ); HRESULT put_AutoPortExtConfig(tagNAAutoPortExtConfig Val ); |
Interface |
IFixturing2 |