Write/Read |
About Auto Port Extensions |
Description |
Enables and disables automatic port extensions on the specified port. All enabled ports will have their reference plane automatically adjusted after performing Automatic Port Extension. |
VB Syntax |
fixture.AutoPortExtState (port) = bool |
Variable |
(Type) - Description |
|
fixture |
A Fixturing (object) |
|
port |
(Integer) Port number to enable or disable. |
|
bool |
(Boolean) True - Enables Auto Port Extensions False - Disables Auto Port Extensions |
Return Type |
Boolean |
Default |
False |
Examples |
fixture.AutoPortExtState(1) = True |
|
value = fixture.AutoPortExtState(2) 'Read |
|
C++ Syntax |
HRESULT get_AutoPortExtState(short port, VARIANT_BOOL *pState ); HRESULT put_AutoPortExtState(short port, VARIANT_BOOL bVal); |
Interface |
IFixturing2 |