Write/Read |
About Balanced Measurements |
Description |
Sets and returns whether the balanced transform is ON or OFF |
VB Syntax |
balMeas.BalancedMode = value |
Variable |
(Type) - Description |
|
balMeas |
A BalancedMeasurement (object) |
|
value |
(Boolean) - State of balanced transform. Choose from False Balanced Transform OFF True Balanced Transform ON |
Return Type |
Boolean |
Default |
False |
Examples |
balMeas.BalancedMode = True 'Write variable = balMeas.BalancedMode 'Read |
C++ Syntax |
HRESULT get_BalancedMode(VARIANT_BOOL *bVal) HRESULT put_BalancedMode(VARIANT_BOOL newVal) |
Interface |
IBalancedMeasurement |