Read-only |
About Spectrum Analyzer Markers |
Description |
Returns the band power level from the band power marker. |
VB Syntax |
value = mkr.BandPowerdBm |
Variable |
(Type) - Description |
|
value |
Variable to store the returned Y-axis power value. |
|
mkr |
A Marker (object) |
Return Type |
Double |
Default |
Not Applicable |
Examples |
value = mkr.BandPowerdBm 'Read |
C++ Syntax |
HRESULT get_BandPowerdBm(double* pVal) |
Interface |
IMarker7 |