Write/Read |
About SA Application |
Description |
Set and read the resolution bandwidth shape. |
VB Syntax |
sa.BandwidthShape = value |
Variable |
(Type) - Description |
|
sa |
A SpectrumAnalyzer (object) |
|
value |
(Enum as NASABandwidthShape) Choose from: 0 - naNoWindow 1 - naWindowFlatTop 2 - naWindowGaussian 3 - naWindowBlackman 4 - naWindowKaiser |
Return Type |
Enum |
Default |
2 - naWindowGaussian |
Examples |
sa.BandwidthShape = naWindowFlatTop 'Write |
|
value = sa.BandwidthShape 'Read |
|
C++ Syntax |
HRESULT put_BandwidthShape(tagNASABandwidthShape shape); HRESULT get_BandwidthShape(tagNASABandwidthShape* shape); |
Interface |
ISpectrumAnalyzer |