Read/Write |
About Embedded LO |
Description |
Sets and returns the frequency span for the broadband tuning sweep. |
VB Syntax |
obj.BroadbandTuningSpan = value |
Variable |
(Type) - Description |
|
obj |
An EmbeddedLO (object) or A ConverterEmbeddedLO (object) |
|
value |
(Double) Broadband frequency span in Hz. |
Return Type |
(Double) |
Default |
3 MHz |
Examples |
embedLO.BroadbandTuningSpan = 1E6 'write |
|
value = embedLO.BroadbandTuningSpan 'read |
|
C++ Syntax |
HRESULT get_BroadbandTuningSpan(double* span); HRESULT put_BroadbandTuningSpan(double span); |
Interface |
IEmbededLO |