Write/Read |
About Markers |
Description |
Sets or returns the bucket number (data point) for the active marker. When the markers are interpolated (non-discrete), the returned value is the nearest marker bucket position. |
VB Syntax |
mark.BucketNumber = value |
Variable |
(Type) - Description |
|
mark |
A Marker (object) |
|
value |
(long integer) - Data point. Choose any number between 0 and the measurement's number of data points - 1. For example, with Number of points = 201, choose between 0 and 200 |
Return Type |
Long Integer |
Default |
The first marker is set to the middle of the span. Subsequent markers are set to the bucket number of the previously active marker. |
Examples |
mark.BucketNumber = 100 'moves the active marker to data point 100 -Write |
|
pointNumber = mark.BucketNumber 'returns the data point number of the marker object. When the markers are interpolated (non-discrete), the returned value is the nearest marker bucket position. |
|
C++ Syntax |
HRESULT get_BucketNumber(long *pVal) |
Interface |
IMarker |