Read/Write |
About Dynamic Uncertainty |
Description |
Sets and returns the ON/OFF state of allowing cable repeatability data to contribute to the uncertainty of a calibration performed using Dynamic Uncertainty. Repeatability data must also be present for the ports at the time the calibration is performed. |
VB Syntax |
uncertMan.CableRepeatabilityEnabled = value |
Variable |
(Type) - Description |
|
uncertMan |
An UncertaintyManager Object |
|
value |
(Boolean) Enable state. Choose from: True - Cable repeatability uncertainty ON. False - Cable repeatability uncertainty OFF. |
Return Type |
Boolean |
Default |
True |
Examples |
uncertMan.CableRepeatabilityEnabled = True |
C++ Syntax |
HRESULT get_CableRepeatabilityEnabled([out,retval] VARIANT_BOOL* pState); HRESULT put_CableRepeatabilityEnabled([in] VARIANT_BOOL state); |
Interface |
IUncertaintyManager |