Write/Read |
About Dynamic Uncertainty |
Description |
Sets and returns the name of the cable that is assigned to the port object for Dynamic Uncertainty. |
VB Syntax |
port.Cable = value |
Variable |
(Type) - Description |
|
port |
A Port (object) |
|
value |
(String) - Cable name. |
Return Type |
String |
Default |
Not Applicable |
Examples |
port.Cable = "MyNewCable" 'Write the value |
C++ Syntax |
HRESULT get_Cable([out,retval] BSTR *pCableName); HRESULT put_Cable([in] BSTR cableName); |
Interface |
IPort |