Read-only |
|
Description |
Returns the stimulus value of the center data point for the measurement. This function does NOT work for segment sweep measurements. To understand how this property is useful, see IMeasurement2 Interface. |
VB Syntax |
value = meas.Center |
Variable |
(Type) - Description |
|
value |
(Double) - Variable to store the returned value. |
|
meas |
A Measurement (object) |
Return Type |
Double |
Default |
Not Applicable |
Examples |
Print meas.Center 'prints the center data point |
C++ Syntax |
HRESULT get_Center(double * Val); |
Interface |
IMeasurement2 |