Read-only |
About Path Configurator |
Description |
Returns an array of stored configuration names that can be used with DeleteConfiguration Method and.LoadConfiguration Method |
VB Syntax |
names = pathMgr.Configurations |
Variable |
(Type) - Description |
|
names |
(Variant array) Variable to store the returned configuration names. |
|
pathMgr |
PathConfigurationManager (object) |
Return Type |
Variant array |
Default |
Not Applicable |
Examples |
names = path.Configurations |
C++ Syntax |
HRESULT get_Configurations (VARIANT* configurations ); |
Interface |
IPathConfigurationManager |