Read-only |
About Cal Sets |
Description |
Returns the Cal Types from the calset. Learn more about Cal Type. |
VB Syntax |
value = calSet.ContentDescriptor |
Variable |
(Type) - Description |
|
calSet |
A CalSet (object) |
Return Type |
1-dimensional variant array |
Default |
Not Applicable |
Examples |
Set app = CreateObject("AgilentPNA835x.Application") Set calset = app.GetCalManager.CalSets.Item(2) desc = CalSet.ContentDescriptor For i = 0 to UBound(desc) MsgBox (desc(i)) Next |
C++ Syntax |
HRESULT get_ContentDescriptor (VARIANT* vals) |
Interface |
ICalSet8 |