Write/Read |
About Phase Control |
Description |
Sets and returns whether to couple phase control settings (IFBW, Tolerance, Max Iterations). |
VB Syntax |
phase.CouplePhasePortSettings(srcPort) = value |
Variable |
(Type) - Description |
|
phase |
A PhaseControl Object |
|
srcPort |
(Long Integer) Source port for which to make phase control settings. Note: If the source port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model, then use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port |
value |
(Boolean) Coupling state. Choose from: True - Couple phase control settings. The phase control settings from <port> are copied to the other phase-controlled ports. False - Do NOT couple phase control settings. The phase control settings for each phase-controlled port are made independently. |
Return Type |
Boolean |
Default |
False |
Examples |
phase.CouplePhasePortSettings 1 = True ' Write |
|
value = phase.CouplePhasePortSettings 2' Read |
|
C++ Syntax |
HRESULT get_CouplePhasePortSettings(long port, VARIANT_BOOL* pVal); HRESULT put_CouplePhasePortSettings(long port, VARIANT_BOOL newVal); |
Interface |
IPhaseControl |