Write/Read |
About External DC Devices |
Description |
Sets and returns the maximum output current value of the external DC Source. This command supports Keysight B2900A and N6700 series devices only. |
VB Syntax |
extDC.CurrentLimit (devicename) = value |
Variable |
(Type) - Description |
|
extDC |
A ExternalDCDevice (object) |
|
devicename |
(String) Name of the device. |
|
value |
(Double) Current limit value. |
Return Type |
Double |
Default |
0 |
Examples |
extDC.CurrentLimit("myDCDevice") = 4 'Write |
|
Limit = extDC.CurrentLimit("myDCDevice") 'Read |
|
C++ Syntax |
HRESULT get_CurrentLimit(BSTR devicename, double *cLimit) |
Interface |
IExternalDCDevice2 |