Write/Read |
About Ext DC Devices |
Description |
Sets and returns the offset correction value for an external DC Device which can be configured as either a DC Meter or a DC Source. |
VB Syntax |
extDC.DCOffset = value |
Variable |
(Type) - Description |
|
extDC |
An ExternalDCDevice (object) |
|
value |
(Double) DC offset value. The VNA will display readings from a DC Meter as: Display = (Meas'd value - Offset) * Scale The VNA will adjust the output from a DC Source as: Output = (Set value - Offset) * Scale |
Return Type |
Double |
Default |
0 |
Examples |
extDC.DCOffset = 4 'Write |
|
offset = extDC.DCOffset 'Read |
|
C++ Syntax |
HRESULT get_DCOffset (double *pValue) HRESULT put_DCOffset (double newVal) |
Interface |
IExternalDCDevice |