Write/Read |
About Ext DC Devices |
Description |
Sets and returns the scale correction value for an external DC Device which can be configured as either a DC Meter or a DC Source. |
VB Syntax |
extDC.DCScale = value |
Variable |
(Type) - Description |
|
extDC |
An ExternalDCDevice (object) |
|
value |
(Double) DC scale value. The VNA will display readings from a DC Meter as: Display = (Meas'd value - Offset) * Scale The VNA will adjust the output from a DC Source as: Output = (Set value - Offset) * Scale |
Return Type |
Double |
Default |
1 |
Examples |
extDC.DCScale = -2 'Write |
|
slope = extDC.DCScale 'Read |
|
C++ Syntax |
HRESULT get_DCScale (double *pValue) HRESULT put_DCScale (double newVal) |
Interface |
IExternalDCDevice |