Write/Read |
About SA Application |
Description |
Set and read the ON/OFF state of the DC sources. If ON, the DC sources sweep between their start and stop voltages. |
VB Syntax |
sa.DCSourceSweepState = value |
Variable |
(Type) - Description |
|
sa |
A SpectrumAnalyzer (object) |
|
value |
(Boolean) Choose from: 0 - OFF - DC sweep OFF. 1 - ON - DC sweep ON. |
Return Type |
Boolean |
Default |
0 |
Examples |
sa.DCSourceSweepState = OFF Write |
|
value = sa.DCSourceSweepState 'Read |
|
C++ Syntax |
HRESULT put_DCSourceSweepState(VARIANT_BOOL bEnable); HRESULT get_DCSourceSweepState(VARIANT_BOOL* bEnable); |
Interface |
ISpectrumAnalyzer |