Write/Read |
About Phase Reference Cals |
Description |
Sets and returns the state of de-embedding (reversing) the port 2 coupler. |
VB Syntax |
phaseRef.DeembedCoupler = value |
Variable |
(Type) - Description |
|
object |
PhaseReferenceCalibration (object) |
|
value |
(Boolean) Port 2 couple de-embed state. Choose from: True - Configures the calibration to include additional measurements to de-embed the effects of reversing the coupler. (This is the same as clearing the “Omit Coupler” checkbox.) False - Exclude additional measurements for de-embedding the effects of reversing the coupler. |
Return Type |
Boolean |
Default |
True |
Examples |
phaseRef.DeembedCoupler = True |
|
value = phaseRef.DeembedCoupler 'Read |
|
C++ Syntax |
HRESULT get_DeembedCoupler(VARIANT_BOOL *value) HRESULT put_DeembedCoupler(VARIANT_BOOL value) |
Interface |
IPhaseReference2 |