Write/Read

Delay (pulse) Property


Description

Sets the pulse delay - the amount of time before a new pulse begins.

 VB Syntax

pulse.Delay(n) = value

Variable

(Type) - Description

pulse

A PulseGenerator (object)

n

(Integer) Pulse generator number. Choose from 0 to 4.

Or use PulseGeneratorID to refer to an external pulse generator.

0 is the generator that pulses the ADC.

value

(Double)  Delay value in seconds. Choose a value from about 33ns to about 70 seconds.

Return Type

Double

Default

0

Examples

pulse.Delay(1) = 1ms 'Write

value = pulse.Delay(4) 'Read

C++ Syntax

HRESULT get_Delay(integer pulse, double* delay);

HRESULT put_Delay(integer pulse, double delay);

Interface

IPulseGenerator