Write/Read |
About Auxiliary Triggering |
Description |
Specifies the delay that should be applied by the VNA after the aux trigger input is received and before the acquisition is made. Note: Use on PNA-X ONLY. Other models do NOT have an Aux Input. |
VB Syntax |
auxTrig.Delay = value |
Variable |
(Type) - Description |
|
auxTrig |
An AuxTrigger (object) |
|
value |
(double) - Delay value in seconds. Choose a value between 0 and 3.0 seconds. |
Return Type |
Double |
Default |
Not Applicable |
Exaamples |
auxTrig.Delay = 1.2 'Write 1.2s Delay |
|
value = auxTrig.Delay 'Read the value |
|
C++ Syntax |
HRESULT get_Delay(double *val); HRESULT put_Delay(double val); |
Interface |
IAuxTrigger |