Write / Read |
About Cal Sets |
Description |
Sets or returns the descriptive string assigned to the Cal Set. Change this string so that you can easily identify each Cal Set constructed. |
VB Syntax |
CalSet.Description = value |
Variable |
(Type) - Description |
|
CalSet |
(object) - A Cal Set object |
|
value |
(string) – Description of the Cal Set |
Return Type |
String |
Default |
“CalSet_n” where n is an integer number. |
Examples |
CalSet.Description = "My Cal Set" 'Write |
C++ Syntax |
HRESULT get_Description(BSTR *pVal) HRESULT put_Description(BSTR newVal); |
Interface |
ICalSet |