Write/Read |
About External Devices |
Description |
Sets and returns the DeviceType for the external device. |
VB Syntax |
extDevices.DeviceType = value |
Variable |
(Type) - Description |
|
extDevices |
An ExternalDevice (object) |
|
value |
(String) Device Type. "Source" - external source "Power Meter" - power meter "DC Meter" - DC voltmeter "DC Source" - DC power supply "Pulse Generator" - external pulse generator |
Return Type |
String |
Default |
"Unknown" |
Examples |
extDevices.DeviceType = "source" Write value = extDevices.DeviceType 'Read See example program to configure PMAR device See example program to configure External Source |
C++ Syntax |
HRESULT get_DeviceType( BSTR* value); HRESULT put_DeviceType( BSTR newVal); |
Interface |
IExternalDevices |