Write/Read |
About Fixturing |
Description |
Sets the differential matching circuit type. To select a user-defined circuit, specify IN ADVANCE the 2-port touchstone filename with DiffPortMatch_UserFilename Property. If you do not specify the appropriate file and you select USER, an error occurs and naNO_CIRCUIT is automatically selected. |
VB Syntax |
fixture.DiffPortMatchMode(pNum) = value |
Variable |
(Type) - Description |
|
fixture |
A Fixturing (object) |
|
pNum |
(Integer) Balanced (logical) port number. Choose from logical ports 1, 2, or 3. Learn more about logical ports. |
|
value |
(Enum as NADiffPortMatchCircuitMode) Choose from: 0 or naSHUNT_L_SHUNT_C_CIRCUIT - Specifies the circuit that consists of shunt L and shunt C. 1 or naUSER_FILE_CIRCUIT - Specifies the user-defined circuit. 2 or naNO_CIRCUIT - Specifies no-circuit. |
Return Type |
Enum |
Default |
naSHUNT_L_SHUNT_C_CIRCUIT |
Examples |
fixture.DiffPortMatchMode(2) = naNO_CIRCUIT 'Write |
|
value = fixture.DiffPortMatchMode(1) 'Read |
|
C++ Syntax |
HRESULT get_DiffPortMatchMode( short port, tagNADiffPortMatchCircuitMode *eVal) HRESULT put_DiffPortMatchMode( short port, tagNADiffPortMatchCircuitMode eVal) |
Interface |
IFixturing2 |