Write/Read |
About Fixturing |
Description |
Sets the Conductance value of the differential matching circuit. |
VB Syntax |
fixture.DiffPortMatch_G(portNum) = value |
Variable |
(Type) - Description |
|
fixture |
A Fixturing (object) |
|
portNum |
(Integer) Balanced (logical) port number. Choose from logical ports 1, 2, or 3. Learn more about logical ports. |
|
value |
(Double) Conductance value in siemens. Choose a value between -1E18 to 1E18. |
Return Type |
Double |
Default |
0 |
Examples |
fixture.DiffPortMatch_G(2) = 1e-3 'Write |
|
value = fixture.DiffPortMatch_G(1) 'Read |
|
C++ Syntax |
HRESULT get_DiffPortMatch_G( short portNum, double *pVal) |
Interface |
IFixturing2 |