Write/Read |
About Fixturing |
Description |
Sets the real part of the impedance value for the differential port impedance conversion function. |
VB Syntax |
fixture.DiffZConvPortReal(portNum) = value |
Variable |
(Type) - Description |
|
fixture |
A Fixturing (object) |
|
portNum |
(Integer) Balanced (logical) port number. Choose from logical ports 1, 2, or 3. Learn more about logical ports. |
|
value |
(Double) Real part of the Impedance value. Choose a value between 0 and 1E18 |
Return Type |
Double |
Default |
See Differential Port Z Conversion Default |
Examples |
fixture.DiffZConvPortReal(2) = 75 'Write |
|
value = fixture.DiffZConvPortReal(1) 'Read |
|
C++ Syntax |
HRESULT get_DiffZConvPortReal( short portNum, double *pVal) |
Interface |
IFixturing2 |