Write/Read |
About FOM |
Description |
Sets or returns the range to be displayed on the VNA x-axis. All traces in the channel have this same x-axis scaling. |
VB Syntax |
FOM.DisplayRange = value |
Variable |
(Type) - Description |
|
object |
An FOM (object) |
|
value |
(string) - Range to be displayed on the VNA x-axis. Case insensitive. |
Return Type |
String |
Default |
"Receivers" |
Examples |
fom.DisplayRange = "Source" 'sets the x-axis to the frequency range of "source" |
|
disprange = fom.DisplayRange 'Read |
|
C++ Syntax |
HRESULT get_DisplayRange(BSTR *pDspRange) |
Interface |
IFOM |