Write/Read |
About Distance MarkerSettings |
Description |
Specifies the measurement type in order to determine the correct marker distance.
This settings affects the display of ALL markers for only the ACTIVE measurement. |
VB Syntax |
trans.DistanceMarkerMode = value |
Variable |
(Type) - Description |
|
trans |
A Transform (object) |
|
value |
(enum As NADistanceMarkerMode) - Choose from: 0 - naDistanceMarkerModeAuto 1 - naDistanceMarkerModeReflection 2 - naDistanceMarkerModeTransmission |
Return Type |
Enum |
Default |
0 - naDistanceMarkerModeAuto |
Examples |
trans.DistanceMarkerMode = naDistanceMarkerModeReflection 'Write |
|
DMM = trans.DistanceMarkerMode 'Read |
|
C++ Syntax |
HRESULT get_DistanceMarkerMode(tagNADistanceMarkerMode *pVal); HRESULT put_DistanceMarkerMode(tagNADistanceMarkerMode newVal); |
Interface |
ITransform2 |