Read-only |
|
Description |
Returns the domain (frequency,time, power, phase) of the measurement. To understand how this property is useful, see IMeasurement2 Interface. |
VB Syntax |
value = meas.Domain |
Variable |
(Type) - Description |
|
value |
(Enum as NADomainType) - variable to store the returned value 0 - naDomainFrequency 1 - naDomainTime 2 - naDomainPower 4 - naDomainPhase |
|
meas |
A Measurement (object) |
Return Type |
Enum as NADomainType |
Default |
Not Applicable |
Examples |
Print meas.Domain 'prints the value of the domain enum |
C++ Syntax |
HRESULT get_Domain(tagNADomainType * Val); |
Interface |
IMeasurement2 |