Description |
Note: This property is replaced by ECALCharacterizationEx Property. Specifies the characterization data within an ECal module to be used for the calibration. Learn more about ECal User Characterization. |
VB Syntax |
cal.ECALCharacterization(mod) = value |
Variable |
(Type) - Description |
|
cal |
Calibrator (object) |
|
module |
1- ECal module |
|
value |
(Long) – Characterization data within the ECal module to be used for ECal operations. Choose from: 0 – Factory Characterization 1 – UserCharacterization1 2 – UserCharacterization2 3 – UserCharacterization3 4 – UserCharacterization4 5 – UserCharacterization5 |
Return Type |
Long |
Default |
0 - Factory Characterization |
Interface |
ICalibrator2 |