Description |
Note: This command is replaced with CalKitType which sets the ECal module and User Characterization. Specifies the characterization data within an ECal module to be used, and the portion of the VMC calibration. Learn more about ECal User Characterization. |
VB Syntax |
VMC.ECALCharacterization (module,port) = value |
Variable |
(Type) - Description |
|
VMC |
VMCType (object) |
|
module |
(long integer) 1 - ECAL module |
|
port |
(boolean) True - 2-port calibration portion of the VMC False - 1-port (mixer characterization portion of the VMC cal) |
|
value |
(Long) – Characterization data within the ECal module to be used for ECal operations. Choose from: 0 – Factory Characterization 1 – UserCharacterization1 2 – UserCharacterization2 3 – UserCharacterization3 4 – UserCharacterization4 5 – UserCharacterization5 |
Return Type |
Long |
Default |
0 - Factory Characterization |
Examples |
VMC.ECALCharacterization (1,True) = 4 |
C++ Syntax |
HRESULT put_ECALCharacterization( long moduleNumber, long characterization); HRESULT get_ECALCharacterization( long moduleNumber, long* characterization); |
Interface |
IVMCType |