Read/Write |
About ECAL |
Description |
Note: The inherent isolation of the VNA is better than that attained with this command. ONLY use this command when using an external test set, and ONLY using a 8509x ECal module. Specifies whether the acquisition of the ECal calibration should include isolation or not. |
VB Syntax |
cal.ECALIsolation = value |
Variable |
(Type) - Description |
|
cal |
A Calibrator (object) |
|
value |
(boolean) False - Exclude Isolation True - Include Isolation |
Return Type |
Boolean |
Default |
False |
Examples |
Dim oPNA as AgilentPNA835x.Application Dim oCal as Calibrator Set oPNA = CreateObject("AgilentPNA835x.Application", "MachineName") Set oCal = oPNA.ActiveChannel.Calibrator ' Uncomment the following line to have the cal include isolation ' oCal.ECALIsolation = True ' Uncomment the following line to have the cal omit isolation 'oCal.ECALIsolation = False oCal.DoECAL2Port ' Do the cal |
C++ Syntax |
HRESULT put_ECALIsolation ( VARIANT_BOOL bIsolationState ); HRESULT get_ECALIsolation ( VARIANT_BOOL *bIsolationState ); |
Interface |
Calibrator |