Description |
Note: This command is replaced by ECALPortMapEx Specifies which ports of the ECal module are connected to which ports of the VNA for the DoECAL1Port and DoECAL2Port methods when the OrientECALModule property = False. |
VB Syntax |
cal.ECALPortMap = value |
Variable |
(Type) - Description |
|
cal |
A Calibrator (object) |
|
value |
(string) (string) -Format this parameter in the following manner: Aw,Bx,Cy,Dz where
Ports of the module which are not used are omitted from the string. For example, on a 4-port ECal module with
the string would be: A2,B3,D1
DoECAL1Port or DoECAL2Port methods will fail if the port numbers passed to those methods are not in the string of this property and OrientECALModule property = False. |
Return Type |
String |
Default |
Not Applicable |
Examples |
Dim cal As Calibrator |
C++ Syntax |
HRESULT put_ECALPortMap(tagNAECALModule ecalModule, BSTR strPortMap); HRESULT get_ECALPortMap(tagNAECALModule ecalModule, BSTR *strPortMap); |
Interface |
ICalibrator3 |