Write/Read |
About External Sources |
Description |
Sets and reads the state of the modulation control. Modulation control must be ON to control the modulation of an external source. |
VB Syntax |
extSource.EnableModulationControl = value |
Variable |
(Type) - Description |
|
extSource |
An ExternalSource Object (object) |
|
value |
(Boolean) Choose from: 1 - Enable control of external modulation. 0 - Disable control of external modulation. Learn about these settings and about adding an external source. |
Return Type |
Boolean |
Default |
0 |
Examples |
extSource.EnableModulationControl = 1 'Write |
|
value = extSource.EnableModulationControl 'Read |
|
C++ Syntax |
HRESULT put_EnableModulationControl(VARIANT_BOOL bEnable); HRESULT get_EnableModulationControl(VARIANT_BOOL* bEnable); |
Interface |
IExternalSource2 |