Write/Read |
About Power Compensation |
Description |
Adjusts the source power at the specified port by the combined amount of loss through ALL enabled fixturing operations. Use this function to set the power level at the DUT input. Learn more. Note: This command affects ALL measurements on the specified channel. |
VB Syntax |
fixture.EnablePowerCompensation (port) = bool |
Variable |
(Type) - Description |
|
fixture |
A Fixturing (object) |
|
port |
(Integer) Port number to receive power compensation. |
|
bool |
(Boolean) True - Compensate source power False - Do NOT compensate source power |
Return Type |
Boolean |
Default |
False |
Examples |
fixture.EnablePowerCompensation(1) = True |
|
value = fixture.EnablePowerCompensation(2) 'Read |
|
C++ Syntax |
HRESULT get_EnablePowerCompensation(short port, VARIANT_BOOL *pState ); HRESULT put_EnablePowerCompensation(short port, VARIANT_BOOL bVal); |
Interface |
IFixturing5 |