Write/Read |
About Gain Compression |
Description |
Set and read the action which should be taken at the end of the last frequency or power sweep in the measurement. This setting is used to protect a sensitive device from too much power during the sweep retrace. |
VB Syntax |
gca.EndOfSweepOperation = value |
Variable |
(Type) - Description |
|
gca |
A GainCompression (object) |
|
value |
(NAGCAEndOfSweepOperation)
|
Return Type |
Enum |
Default |
naStandard |
Examples |
gca.EndOfSweepOperation = naSetToStartPower 'Write |
|
eos = gca.EndOfSweepOperation 'Read |
|
C++ Syntax |
HRESULT get_EndOfSweepOperation(tagNAGCAEndOfSweepOperation* pVal) HRESULT put_EndOfSweepOperation(tagNAGCAEndOfSweepOperation newVal) |
Interface |
IGainCompression |