Write/Read |
About SA Application |
Description |
Set and read the ADC record size. |
VB Syntax |
sa.ForceADCRecordSize = value |
Variable |
(Type) - Description |
|
sa |
A SpectrumAnalyzer (object) |
|
value |
(Long) Choose a value between 64 and 33554432 |
Return Type |
Long |
Default |
64 |
Examples |
sa.ForceADCRecordSize = 256 'Write |
|
value = sa.ForceADCRecordSize 'Read |
|
C++ Syntax |
HRESULT put_ForceADCRecordSize(long val); HRESULT get_ForceADCRecordSize(long* val); |
Interface |
ISpectrumAnalyzer |