Write/Read |
About SA Application |
Description |
Set and read the LO frequency. |
VB Syntax |
sa.ForceLOToFrequency= value |
Variable |
(Type) - Description |
|
sa |
A SpectrumAnalyzer (object) |
|
value |
(Double) Choose a value within the LO frequency range. |
Return Type |
Double |
Default |
1 GHz |
Examples |
sa.ForceLOToFrequency= 1e9 Write |
|
value = sa.ForceLOToFrequency 'Read |
|
C++ Syntax |
HRESULT put_ForceLOToFrequency(double val); HRESULT get_ForceLOToFrequency(double* val); |
Interface |
ISpectrumAnalyzer |