Write/Read |
About Marker Format |
Description |
Sets (or returns) the format of the marker. |
VB Syntax |
mark.Format = value |
Variable |
(Type) - Description |
|
mark |
A Marker (object) |
|
value |
(enum NAMarkerFormat) - Choose from: 0 - naMarkerFormat_LinMag 1 - naMarkerFormat_LogMag 2 - naMarkerFormat_Phase 3 - naMarkerFormat_Delay 4 - naMarkerFormat_Real 5 - naMarkerFormat_Imaginary 6 - naMarkerFormat_SWR 7 - naMarkerFormat_LinMagPhase 8 - naMarkerFormat_LogMagPhase 9 - naMarkerFormat_RealImaginary 10 - naMarkerFormat_ComplexImpedance 11 - naMarkerFormat_ComplexAdmittance 12 - naMarkerFormat_Kelvin 13 - naMarkerFormat_Fahrenheit 14 - naMarkerFormat_Celsius 15 - naMarkerFormat_Default - the same format as the trace. 16 - naMarkerFormat_Noise - Available ONLY in IM Spectrum and SA measurement classes. |
Return Type |
NAMarkerFormat |
Default |
15 -naMarkerFormat_Default |
Examples |
mark.Format = naMarkerFormat_SWR 'Write |
|
fmt = mark.Format 'Read |
|
C++ Syntax |
HRESULT get_Format(tagNAMarkerFormat *pVal) HRESULT put_Format(tagNAMarkerFormat newVal) |
Interface |
IMarker |