Write/Read |
About Data Format |
Description |
Sets or returns the display format of the measurement. |
VB Syntax |
meas.Format = value |
Variable |
(Type) - Description |
|
meas |
A Measurement (object) |
|
value |
(enum NADataFormat) - Choose from: 0 - naDataFormat_LinMag 1 - naDataFormat_LogMag 2 - naDataFormat_Phase 3 - naDataFormat_Polar 4 - naDataFormat_Smith 5 - naDataFormat_Delay 6 - naDataFormat_Real 7 - naDataFormat_Imaginary 8 - naDataFormat_SWR 9 - naDataFormat_PhaseUnwrapped 10 - naDataFormat_InverseSmith 11 - naDataFormat_Kelvin 12 - naDataFormat_Fahrenheit 13 - naDataFormat_Celsius 14 - naDataFormat_PhasePositive |
Return Type |
Long Integer |
Default |
1 - naDataFormat_LogMag |
Examples |
meas.Format = naDataFormat_Real 'Write |
|
fmt = meas.Format 'Read |
|
C++ Syntax |
HRESULT get_Format(tagDataFormat *pVal) HRESULT put_Format(tagDataFormat newVal) |
Interface |
IMeasurement |