Write/Read |
About Frequency Offset |
Description |
This method is replaced by properties on the FOMRange Object. Enables Frequency Offset on ALL measurements that are present on the active channel. This immediately causes the source and receiver to tune to separate frequencies. The receiver frequencies are specified with other channel and offset settings. To make the stimulus settings, use Channel Start, Stop Frequency properties. See other Frequency Offset properties. Tip: To avoid unnecessary errors, first make other frequency offset settings. Then turn Frequency Offset ON. |
VB Syntax |
object.FrequencyOffsetState = value |
Variable |
(Type) - Description |
|
object |
Channel (object) or CalSet (object) - Read-only property |
|
value |
(Enum as NaStates) - Choose from: naOFF (0) - Turns Frequency Offset OFF naON (1) - Turns Frequency Offset ON |
Return Type |
Enum |
Default |
naOFF (0) |
Examples |
chan.FrequencyOffsetState = naON 'Write |
|
Foffset = chan.FrequencyOffsetState 'Read |
|
C++ Syntax |
HRESULT FrequencyOffsetState (tag NAStates *pState); |
Interface |
IChannel2 |CalSet3 |