Write/Read |
About Group Delay |
Description |
Sets group delay aperture using a fixed frequency range. |
VB Syntax |
gdAperture.Frequency = value |
Variable |
(Type) - Description |
|
gdAperture |
A GroupDelayAperture (object) |
|
value |
(Double) Frequency range (in Hz) to use for the aperture setting. |
Return Type |
Double |
Default |
Frequency range that equates to 11 points. This can be changed to two points with a preference setting. |
Examples |
gdAperture.Frequency = 1e6 'Write |
|
aperture = gdAperture.Frequency 'Read |
|
C++ Syntax |
HRESULT get_Frequency(double Frequency *pVal) HRESULT put_Frequency(double Frequency newVal) |
Interface |
IGroupDelayAperture |