Read-Only |
About External Devices |
Description |
Returns a value indicating whether the specified external devices is configured. |
VB Syntax |
value = extDevices.HasItem(name) |
Variable |
(Type) - Description |
|
value |
(Boolean) Variable to store one of the following returned values. False - Item (name) is NOT present in the External Devices collection. True - Item (name) IS present in the External Devices collection. |
|
extDevices |
An ExternalDevices (collection) |
|
name |
(String) Name of External Device for which to search the collection. |
Return Type |
Boolean |
Default |
Not Applicable |
Examples |
has = extDevices.HasItem('mysource')'Read |
C++ Syntax |
HRESULT get_HasItem( VARIANT Index, BOOL *pVal); |
Interface |
IExternalDevices |