Write/Read |
About Cal All |
Description |
Sets and returns the IFBW for a Cal All calibration. Learn more about this setting. |
VB Syntax |
calAll.IFBW = value |
Variable |
(Type) - Description |
|
calAll |
A CalibrateAllIFBW (object) |
|
value |
(Double) IFBW in Hz. |
Return Type |
Variant |
Default |
1 kHz |
Examples |
calAll.IFBW = 10e3 'sets IFBW to 10 kHz ifbw = calAll.IFBW 'returns the ifbw setting |
C++ Syntax |
HRESULT get_IFBW (Double *Val) HRESULT put_IFBW (Double newVal) |
Interface |
ICalibrateAllChannels |