Write/Read |
About ECal Extrapolation |
Description |
Sets whether a Swept IMD or IMDx calibration can exceed the stop frequency limit of an ECal module. |
VB Syntax |
pref.IMDECalExtrapolation = bool |
Variable |
(Type) - Description |
|
pref |
A Preferences (object) |
|
bool |
(Boolean) - Choose from: False - Do NOT allow extrapolation. True - Allow extrapolation. |
Return Type |
Boolean |
Default |
False |
Examples |
pref.IMDECalExtrapolation = False 'Write |
|
prefer = pref.IMDECalExtrapolation 'Read |
|
C++ Syntax |
HRESULT put_IMDECalExtrapolation( VARIANT_BOOL bExtrap) HRESULT get_IMDECalExtrapolation( VARIANT_BOOL *bExtrap) |
Interface |
IPreferences14 |