Write/Read |
About External Devices |
Description |
Sets and returns the method of communication and address for the external device. |
VB Syntax |
extDevices.IOConfiguration = value |
Variable |
(Type) - Description |
|
extDevices |
An ExternalDevice (object) |
|
value |
(String) Configuration path. Any valid VISA resource shown in the IO Configuration field of the External Devices dialog, enclosed in quotes. Do NOT use the ID string of a PMAR USB power sensor as the resource string. The ID string is returned by the USBPowerMeterCatalog Property |
Return Type |
String |
Default |
" " Empty String |
Examples |
extDevices.IOConfiguration = "TCPIP::141.121.76.239::inst0::INSTR" Write value = extDevices.IOConfiguration 'Read See example program to configure PMAR device See example program to configure External Source |
C++ Syntax |
HRESULT get_IOConfiguration( BSTR* value); HRESULT put_IOConfiguration( BSTR newVal); |
Interface |
IExternalDevices |