Write/Read |
About SA Application |
Description |
Sets and returns the image rejection strength. During the image rejection process, several LO acquisitions overlap at the same RF frequency. As a result, different RF signal values can be returned. This command sets the acceptable power differences between LOs in determining actual signals. |
VB Syntax |
sa.ImageRejectStrength = value |
Variable |
(Type) - Description |
|
sa |
A SpectrumAnalyzer (object) |
|
value |
(enum NASAStrength) - Choose from: 0 naSAWeak: 3 dB (approximate value, depends on RBW) 1 naSANormal: 1 dB (approximate value, depends on RBW) 2 naSAStrong: 0.5 dB (approximate value, depends on RBW) |
Return Type |
Enum as NASAStrength |
Default |
naSANormal |
Examples |
sa.ImageRejectStrength = naSAStrong 'Write |
|
Strength = sa.ImageRejectStrength 'Read |
|
C++ Syntax |
HRESULT get_ImageRejectStrength(tagNASAStrength* pVal) |
Interface |
ISpectrumAnalyzer4 |