Write/Read |
About SMC CalTypes |
Description |
Sets whether to include SC12 sweeps during measurements. |
VB Syntax |
obj.IncludeReverseSweep = bool |
Variable |
(Type) - Description |
|
obj |
A Converter (object) |
|
bool |
(Boolean) - True - Include the SC12 (reverse) sweep. False - Do NOT Include the SC12 (reverse) sweep. |
Return Type |
Boolean |
Default |
True |
Examples |
obj.IncludeReverseSweep = True |
C++ Syntax |
HRESULT get_IncludeReverseSweep(VARIANT_BOOL * val); HRESULT put_IncludeReverseSweep(VARIANT_BOOL val); |
Interface |
IMixer12 |